5G NR

BWP Setup Uplink

The uplink consist of signals that are used for reception and transmission of the channels and the channels themselves that carry the higher level data.

The signals are:

The channels are:

A feature of 5G NR is a Bandwidth Part (BWP). With cells being up to 400-MHz wide, very complex processing would be required to cover the entire bandwidth. BWP is a contiguous set of physical resource blocks (PRBs) on a given carrier. These RBs are selected from a contiguous subset of the common resource blocks for a given numerology (u). Reserved resources can be configured within the BWP and each BWP has its own numerology, that is, subcarrier spacing and cyclic prefix (CP).

Up to four BWPs can be allocated, but only one BWP in the downlink and one in the uplink is active at a given time. Configuration parameters include:

CP is used to mitigate the effects of channel delay spread and intersymbol interference. CP provides a buffer to protect the OFDM signal from inter-symbol interference by repeating the end of the symbol at the start of the same symbol. While this reduces the achievable data rate, it completely eliminates the inter-symbol interference up to the length of the CP. In 5G NR, as subcarrier space changes, the cyclic prefix length also scales accordingly, making it possible to adapt the CP length to the channel conditions.

Add BWP

Delete BWP

Copy BWP

BWP Count

BWP_ID

Name

Numerology

RB Offset (N_BWP_start)

RB Number (N_BWP_size)

Add BWP

Adds a new Bandwidth Part (BWP) to the setup table. BWP setup nodes are required so that each data channel can select which BWP to use. The maximum number of supported BWPs is 16.

See also, Adding, Copying, and Deleting BWP or Channels.

GUI Location

Apps > 5G NR > Carrier > Carrier n (UL) > Uplink > BWP > + (plus symbol)

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:BWP:ADD

SCPI Example

RAD:NR5G:WAV:CCAR0:ULINk:BWP:ADD

Delete BWP

Deletes the selected BWP from the setup table.

See also, Adding, Copying, and Deleting BWP or Channels.

GUI Location

Apps > 5G NR > Carrier > Carrier n (UL) > Uplink > BWP > ... (eclipses symbol) > Delete

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:BWP:DELete <integer>

SCPI Example

RAD:NR5G:WAV:CCAR0:ULINk:BWP:DEL 1

Copy BWP

Copies the currently selected BWP to the last column of the setup table. The maximum number of supported BWPs is 16.

See also, Adding, Copying, and Deleting BWP or Channels.

GUI Location

Apps > 5G NR > Carrier > Carrier n (UL) > Uplink > BWP > ... (eclipses symbol) > Copy

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:BWP:COPY <integer>

SCPI Example

RAD:NR5G:WAV:CCAR0:ULIN:BWP:COPY 1

BWP Count

Displays or queries the number of BWPs configured.

GUI Location

Apps > 5G NR > Carrier > Carrier n (UL) > Uplink > BWP > displays the configured BWPs

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:BWP:COUNt?

SCPI Example

RAD:NR5G:WAV:CCAR0:ULINk:BWP:COUN?

Preset

1

State Saved

No

BWP_ID

Displays the ID of current BWP, it is automatically generated based on the index of the BWP array.

GUI Location

Apps > 5G NR > Carrier UL >Uplink > BWP > BWP ID

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:BWP<bwp>:ID?

SCPI Example

RAD:NR5G:WAV:CCAR0:ULINk:BWP0:ID?

Preset

0 | 1 | 2 | 3 | 4 | 5 | 6 | 7

State Saved

Yes

Name

Displays the auto-filled, read-only name of the BWP. It is used to select the BWP for the data channel.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > BWP > Name

Numerology

Specifies the numerology used by the BWP. Numerology specifies the subcarrier spacing and cyclic prefix definition used for this bandwidth part. Numerology affects symbol duration and the number of subcarriers possible for a given carrier bandwidth.

When Cell-Specific > Numerology Mode is set to Single Numerology, the BWPs numerology setting is coupled to the value set in the Carrier (Cell-Specific) numerology.

When Cell-Specific > Numerology Mode is set to Multiple Numerologies, a Resource Grid tab is added to the bottom pane of the GUI where you can select one to three numerologies for the selected Bandwidth.

For FR1, the choices are: 15 kHz, 30 kHz, or 60 kHz.

For FR2, the choices are: 60 kHz, 120 kHz, and 240 kHz.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > BWP > Numerology

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:BWP<bwp>:NUMerology MU0|MU1|MU2Ncp|MU2Ecp|MU3|MU4

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:BWP<bwp>:NUMerology?

SCPI Example

RAD:NR5G:WAV:CCAR0:ULINk:BWP1:NUM MU0

RAD:NR5G:WAV:CCAR0:DLINk:BWP1:NUM?

Couplings

Coupled with Numerology Mode and Numerology Enable of resource grid and carrier numerology.

When Numerology Mode is single mode, this setting’s value will be coupled to be same with carrier numerology.

When Numerology Mode is multiple mode, the value ranges of this setting are those Numerology Enable of resource grid being enabled except MU2Ncp|MU2Ecp.

For example if Numerology Enable of resource grid with numerology 0 and 1 are enabled, then this setting’s value range will be u = 0: 15 kHz | u = 1: 30 kHz.

When current value of this setting is not in the valid value ranges, this setting will be coupled to the valid value automatically.

For initial BWP

   Auto Configuration == On

       Numerology Value is determined by MIB subcarrierSpacingCommon (RMSI-scs), and subcarrierSpacingCommon also has other dependencies.

       subcarrierSpacingCommon = 15kHz => μ = 0 : 15kHz

       subcarrierSpacingCommon = 30kHz => μ = 1 : 30kHz

       subcarrierSpacingCommon = 60kHz => μ = 2 : 60kHz Normal CP

       subcarrierSpacingCommon = 120kHz => µ = 3: 120 kHz

Auto Configuration == Off

    SingleNumerology Mode

          Numerology value = carrier Numerology value.

    MultiNumerology Mode

            Numerology choices: those being enabled resource grids

           For example if Numerology Enable of resource grid with numerology 0 and 1 are enabled, then this setting’s value range will be u = 0: 15 kHz | u = 1: 30 kHz.

Non-initial BWP

   SingleNumerology Mode

          Numerology value = carrier Numerology value.

    MultiNumerology Mode

          Numerology choices: those being enabled resource grids

Preset

MU1

State Saved

Yes

RB Offset (N_BWP_start)

Sets the RB offset of the current bandwidth part (BWP) relative to CRB0.

A resource block (RB) consists of 12 contiguous subcarriers. The RB Number determines the contiguous amount of spectrum available to the specified BWP, starting from the RB Offset within the containing component carrier. The maximum number of RBs potentially available to this BWP is determined by the numerology of this BWP and the maximum RB limit specified for the component carrier for that particular numerology.

GUI Location

Apps > 5G NR > Carrier UL > Uplink > BWP > RB Offset (N_BWP_start)

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:BWP<bwp>:RB:OFFSet <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:BWP<bwp>:RB:OFFSet? [MAXimum|MINimum]

SCPI Example

RAD:NR5G:WAV:CCAR0:DLINk:BWP1:RB:OFFS 3

RAD:NR5G:WAV:CCAR0:DLINk:BWP1:RB:OFFS?

Couplings

For Initial BWP, if Auto Configuration is ON, this setting cannot be set and the value is calculated automatically.

For BWP1 , this setting is settable and readable.

The maximum value of this setting couples with Numerology Mode and resource grid defined in carrier

Preset to 126 for Initial BWP

Preset to 0 for other BWPs.

Preset

126 | 0 | 0 |0 | 0 | 0 | 0 |0

State Saved

Yes

Min

0

Max

272

Resolution

1

RB Number (N_BWP_size)

Set the resource block (RB) number of the bandwidth part (BWP).

GUI Location

Apps > 5G NR > Carrier UL > Uplink > BWP > RB Number (N_BWP_size)

SCPI Command

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:BWP<bwp>:RB:NUMBer <integer>

[:SOURce]:RADio:NR5G:WAVeform[:ARB]:CCARrier<carrier>:ULINk:BWP<bwp>:RB:NUMBer? [MAXimum|MINimum]

SCPI Example

RAD:NR5G:WAV:CCAR0:ULINk:BWP1:RB:NUMB 100

RAD:NR5G:WAV:CCAR0:ULINk:BWP1:RB:NUMB?

Couplings

For Initial BWP, if Auto Configuration is On, this setting cannot be set and the value is calculated automatically.

For BWP1, this setting is settable and readable.

Preset

24 | 273 | 273 |273 | 273 | 273 | 273 |273

State Saved

Yes

Min

1

Max

273

Resolution

1

Carrier Uplink